230 Volt Relay output module for SE7000 controllers

Issue

Sometimes, switching 230V with the SE7000 controller is requested and/or necessary, but no such product is listed in the current portfolio.

Product Line

Field Devices, SmartStruxure Lite

Environment

SE7000 series controllers

Cause

No product that matches the requests are currently listed in the portfolio

Resolution

Two relay boards for fan coil units will be released late 2012.  These will allow the SE7000 devices to be used with 230V systems.