Preset 95: Accessing Esprit Main Menu

Issue

Cannot call up the Esprit main menu on the monitor by entering preset 95.

Product Line

Pelco Cameras, Pelco Video Management, Pelco Matrix

Environment

  • Esprit positioning system
  • CM6700/CM6800
  • KBD200A/KBD300A: Direct Mode
  • CM9500
  • CM9740/CM9760/CM9770/CM9780
  • KBD4000/KBD4002/KBD4000V
  • MPT9500
  • Endura Workstation (WS)
  • VCD5000

Cause

Programming preset 95 for Pelco's controllers varies according to the type of controller you are using.

Resolution

Below are instructions for programming preset 95 for various Pelco controllers.

NOTE: (use preset 28 in AD32-preset mode.)

CM6700/CM6800

  1. Enter the number of the Esprit system and press the CAM key.
  2. Enter 95 and hold the PRESET key for two seconds.
  3. In the Edit Preset menu, go to SET and press the ACK key. The main menu appears.

KBD200A/KBD300A: (Direct Mode Only)

  1. Enter 95
  2. Hold the PRESET key (approximately five seconds) until the main menu appears on the screen.

CM9500

  1. Enter the number of the Esprit system and press the CAM key. The main menu appears.
  2. Highlight SETUP in the main menu and press the SELECT key.
  3. Highlight CAM in the Setup menu and press the SELECT key.
  4. Highlight PRESET in the Camera menu and press the SELECT key.
  5. Enter 95 and press the F1 key. The main menu appears.

CM9740/CM9760/CM9770/CM9780

  1. Press the ESCAPE key to open the main menu. Select DEF. The Define submenu appears.
  2. Enter your four-digit PIN if this is your first time entering this mode.
  3. Enter 95 and select PRST. The main menu appears on the monitor.
  4. Select the Quit icon to return to the default menu.

KBD4000/KBD4002/KBD4000V

  1. Press the SPOT MONITOR key.
  2. Enter 95, then hold the PRESET key (approximately five seconds) until the main menu appears on the screen.

MPT9500
Standard Coaxitron Mode

  1. Enter 95 and press the PRESET SET key.
  2. Position the asterisk in the YES row and press the F1 key. The main menu appears.

Extended Coaxitron or RS-485 Mode

  1. Enter 95 and press the PRESET SET key.
  2. Press the F2 key. The main menu appears.

Endura Workstation

  1. Right-click in the video pane of the Esprit system.
  2. Click Preset and then click Select Preset.
  3. Enter 95 and then click OK.

VCD5000

  1. Select a video pane that is displaying video from an Esprit positioning system.
  2. Enter 95 for the preset action. The shortcuts menu appears.
  3. Press the Preset button on the KBD5000.