LonWorks on an AS and replacing the template without deleting devices

Issue

LonWorks on an AS and replacing the template without deleting devices

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site with LonWorks interface

Cause

Site would like to replace the XIF template without deleting devices

Resolution

Unfortunately there is no way to replace the template without removing all devices. Even if the site is fully commissioned and devices are installed, the site must be re-commission and bind everything again. The template cannot be replaced without deleting the devices installed.