Issue
It is possible to create a receiver group in XBuilder that can be edited by the customer through the web browser. This will allow the customer to make changes without downloading a new project to the controller.
Environment
- Xenta Server
- Xenta 511, 511:B, 527, 701, 711, 721 and 731
- XBuilder
Cause
Edit receiver groups using your web browser
Resolution
It is possible to create a page that will allow your customer to view and edit the receiver group from the web page without using XBuilder.
- Create the receiver group in the system pane of XBuilder
- Create a new Edit Alarm Page in the system pane of XBuilder
- Drag and drop the receiver group onto the new Edit Alarm Page
Once this connection is made, the receiver group will be displayed on the Edit Alarm Page when the customer logs onto the controllers' website.