TAC Xenta 102-AX TGML plug-in for StruxureWare Building Operation

Issue

There is no quick and efficient way to configure a TAC Xenta 102-AX controller after adding it to a LonWorks Network in StruxureWare Building Operation.

Product Line

SmartStruxure Solution

Environment

  • Workstation

Cause

The TAC Xenta 102-AX controller is typically configured using a LNS plug-in that is currently not available in version 1.4.0 and newer.

Resolution

As an alternative to the LNS plug-in this graphic page can be used. The TAC Xenta 102-AX TGML plug-in can be downloaded here off of the Schneider Electric Community website. This zip file contains the TGML graphic, binding template, and a full import file with a Xenta 102-AX that is already bound.