Issue
These Infinet controllers either in limited production or no longer manufactured, but are they supported?
Environment
CyberStation
Cause
Upgrade from Continuum 1.62 is desired. Are LCX898 and ACX781 still supported?
Resolution
Yes, they are supported in all CyberStation versions from v1.62 to 1.94
with no chip change required