Using Spectra IV TXB-N sometimes settings do not take the first time in Endura

Issue

When using Endura doing brightness or other video settings on the Spectra IV TXB-N, the settings will not always take the first time

Product Line

Pelco Cameras, Pelco Video Management

Environment

Endura

Spectra IV with TXB-N h264

Cause

Endura doesn't always register the brightness or other video settings in the TXB-N the first time they are type it to set up

Resolution

If you type the settings in a second time they should take without any problems