How many IO Modules can fit in the universal enclosures?

Issue

Panel layout.

Product Line

Andover Continuum

Environment

 ERG-UNIV-ENC-1

ERG-UNIV-ENC-2

Cause

Need to determine panel layout for a project using the universal enclosures.

Resolution

From the data sheet...

Medium Enclosure:
Andover Continuum Power Supply and NetController, and up to two I/O modules or up to six I/O modules or CX 9702 SiteController.
 

Small Enclosure:
Up to three I/O modules or CX 9702 SiteController or NetController (without a Power Supply) or VS-8-4 Video Switch Module.

Both units are designed to hold two standard 12 VDC 7AH lead acid batteries (not provided).

See the full data sheet here.