Issue
Must add XDriver to a CX9200 where all other ports are being used.
Environment
- xdriver
- Comm Port
- CX9200
- CX9300
Cause
As soon as the port mode switches from xdriver to some other mode the xdriver file is detached and must be reattached to the comm port for the xdriver to work.
Resolution
The default mode of a comm port that is being used with an xdriver must be hard set to xdriver.