Issue
Can an Infinity Controller with a Modbus xdriver operate as a slave node to a third party Modbus device that is set up as the master node?
Environment
Modbus RTU
Modbus TCP/IP
xdriver
Cause
Third party modbus Master has to poll data from a CX or BCX controller that is set up as a slave node.
Resolution
The Modbus TCP/IP xdriver can be configured to operate as a slave node.
The Modbus RTU xdriver must be the Master node whatever MODbus network it is attached to.