Periodic Report is not printed

Issue

Periodic Report is not printed.

Product Line

TAC Vista

Environment

TAC Vista 5.1.7

Cause

If the box "Automatically set printing area" is checked in the properties for the report, the report is not printed. If it is left unchecked, the report will print.

Resolution

Uncheck the box "Automatically set printing area" in the properties for the report .