Issue
Need replacement for AVUM4601 valve actuator
Environment
VEU, MEU, FEU, VZX, MZX
Cause
Need replacement for AVUM4601, AVUE4304, AVUE4354 or AVUX4202 valve actuator
Resolution
Use AVUM5601 actuator, this is the replacement for AVUM4601 230Vac actuator
Also
AVUE4304 is replaced by AVUE5304
AVUE4354 is replaced by AVUE5354
AVUX4202 is replaced by AVUX5202
Click HERE for the datasheet
Click HERE for the Installation Instructions