How to Upgrade the firmware of the AS

Issue

Upgrade the AS to the latest  firmware 

Product Line

SmartStruxure Solution

Environment

Windows 

SmartStruxure

Cause

Need instructions on how to Upgrade AS firmware

Resolution

Upgrading the firmware of the AS

Steps:

  1. At first, make sure you disconnect the USB cable and us the ethernet connection as it is a faster way to upgrade the AS
  2. In the Device Administrator click "Add Network Automation Server"  
  3. Write the ip address you just gave at the first line - OK
  4. You should be able to see something like this:

  5. Click the Upgrade Device(s) button      and this will appear:

  6. Click OK to start the process
  7. After a while, you should get "Install finished successfully!" to the Upgrade status column

Now you can close the StruxureWare Device Administrator