Issue
How to create 0-10Vdc or 0/4-20mA Analogue Input on a 532 Controller
Environment
- Analogue Input
- 532
Cause
How to create 0-10Vdc or 0/4-20mA Analogue Input on a 532 Controller?
Resolution
On the 532 there are 2 rows of links.
The left hand row need to be unlinked i.e. set for non-resistive.
The right hand row needs to be set for AI with the middle and right hand pin linked.
Next the input needs to be modified with resistors as follows:
0-10Vdc
0/4-20mA