Issue
A repair of the power and communication boards for the LCM-84000 and GCM-84000 is being considered. Before contacting the repair company, the part numbers are needed to reference the right boards. What are the part numbers?
Environment
Network 8000
LCM-84000
GCM-84000
Cause
Existing boards in disrepair.
Resolution
The part numbers are as follows:
LCM
power card - part# LCMA-103 (referred to as the UIO or Universal Input Output card)
communication card - part# LCMA-116
GCM
power card - part# GCMA-106 (referred to as the SIO or Serial Input Output card)
communication card - part# GCMA-105