UDI5000-MTRX v9700 PSM File location.

Issue

There is no export area in the UDI5000-MTRX for your PSM file while in v9700 mode.

Product Line

Pelco Video Management

Environment

UDI5000-MTRX 2.0 and higher using v9700 mode.

Cause

The UDI5000-MTRX in v9700 mode uses a PSM for programming. If a customer loses his PSM file and wants to export the current running PSM out of his UDI5000-MTRX, he can perform the following.

Resolution

The location of the PSM file on the UDI5000-MTRX is /usr/local/Pelco/conf/endura.psm. To copy this file from the UDI5000 to your local computer, follow these steps:

  1. Open Endura Utilities.
  2. Log in as admin.
  3. On the left side, select UDI5000-MTRX.
  4. Right click on your primary UDI5000-MTRX that is running in v9700 mode.
  5. Select SCP > Copy Files From.
  6. In the remote path, type in
    /usr/local/Pelco/conf/endura.psm
  7. For the destination select the DESKTOP.
  8. When it is complete, there will be a folder on your desktop titled with the IP of the UDI5000-MTRX.
  9. Open the newly created folder and you will see a file called endura.psm which is your active running PSM file.