How to identify what ports are being used on a PC

Issue

How to identify what ports are being used on a PC

Product Line

TAC I/NET, TAC Vista, Andover Continuum, Satchwell MicroNet, Satchwell Sigma, TAC I/A Series, Field Devices, SmartStruxure Solution, Other, Pelco Cameras, Pelco Monitors, Pelco Video Management, Pelco Matrix, Pelco Transmission & Power

Environment

Any Windows OS

Cause

Running multiple applications  on the same PC  without managing TCP/UDP port assignments can lead to conflicts.

Resolution

TCPView will help you identify all ports and services to each application.

Download from Microsoft's website http://technet.microsoft.com/en-us/sysinternals/bb897437.aspx

Detailed instructions are available at the site.