Issue
Server does not exist or access denied error when using Continuum DB Initialization.
All settings appear to have correct values but the DB initialization fails with the error mentioned above.
Environment
CyberStation
SQL Server
Cause
Multiple instances of SQL server installed in the server machine.
Resolution
When multiple instances of SQL are installed in the server the instance MUST be specified along with the server name.
Example: In the Server Name field of Database Initialization Server window type:
SERVER_MACHINE_NAME\SQL2008
not just SERVER_MACHINE_NAME