Pinpoint crashes when jumping between Graphic panels.

Issue

Pinpoint crashes when jumping between Graphic panels. This then causes the other modules to eventually crash and Continuum needs to be exited un-graciously then restarted.

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Pinpoint

Cause

Too many active data links on the Graphics panels for the Pinpoint engine to deal with.

Resolution

Reduce the number of active data links to 100 or less per Graphic panel. For stability, this is the recommended maximum number of active data links that one Graphic panel can support.