MR 160 resets every minute

Issue

MR 160 resets every minute. It is the only sub-LAN controller resetting. Replacing the hardware has no effect on the resetting issue.

Product Line

TAC I/NET

Environment

MR160

Cause

Station conflicts can cause this behavior. The MR 160 is unique in that it uses two consecutive addresses on the subLAN and is designed for inputs only. The MR 160 provides no output points or MR-resident DDC modules.

Resolution

  1. Make sure there are no station address conflicts.
  2. Make sure the database has not violated the specifications for inputs only.
  3. Refer to TCON 126 for more information.