Sigma - What SAP code is used to purchase Sigma Light, the 400 object edition.

Issue

Purchasing Sigma Light.

Product Line

Satchwell Sigma

Environment

Sigma Light

S-400

SAP code

Cause

There are two options available.

Resolution

On SAP there are two options available.

  1. ZS_Ver_S-400, which should be used when ordering software for a new site.
  2. ZSO_Ver_S-400, which should be used when a customer wishes to upgrade from Sigma Light to Sigma full.