PIR functionality/ordering options SE7300 series controllers

Issue

What is included when the PIR option is ordered?

Product Line

TAC Vista, Andover Continuum, Satchwell Sigma, TAC I/A Series, Field Devices, SmartStruxure Solution, SmartStruxure Lite

Environment

SE7300 series controllers

Cause

The SE7300 series controllers can be ordered both with and without the PIR option

Resolution

If the PIR sensor functionality is ordered as included from factory, code 55 (example: SE7600A5545E) should be used.

If PIR functionality is not required, code 50 (example: SE7600A5045E) should be used.

PIR functionality can be retrofit at any time. For details and part numbers, please see related documentation.