How to set the IP address on a DX4500/4600 DVR.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Setting the IP address on the DX4500/4600 DVR.

Product Line

Pelco Video Management

Environment

  • DX4500
  • DX4600

Cause

Setting the IP address on a DX4500/4600 DVR.

Resolution

1. Log in as the admin.

2. Click on the gear (icon) in the tool bar to get into setup screens.

3. Click on the Network (icon).

    Leave DHCP (On) if you are using a DHCP server and not using static addressing.

4. To add a static IP address turn off "DHCP".

5. Add the static IP address, subnet mask and gateway then click on "exit"

Configuration data is Changed and a save new settings window will pop up, click ok.