Can Infinet controllers share information when there is no Network level controller?

Issue

Can an i2920 and an i2857 be used together without a CX controller?

Product Line

Andover Continuum

Environment

  • Infinet
  • Stand Alone
  • i2

Cause

Want to install a control system without a Netcontroller.

Resolution

Infinet controllers that reside on the same infinet bus are able to share data when the parent Infinity controller is offline or removed from the bus.