Is the DX45/4600 Client MAC compatible.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Is the DX45/4600 Client MAC compatible.

Product Line

Pelco Video Management

Environment

  • DX4500/DX4600
  • DX4500/DX4600 Client

Cause

The DX4500/4600 Client program is not compatible with a Mac OS.

Resolution

At this time the DX4500/4600 client will not run on a Mac OS . Here are the PC requirements. 

REMOTE PC CLIENT APPLICATION

  • Minimum PC Requirement
  • Operating System Windows 2000 (SP4) or later and
  • DirectX ® 8.1 or later
  • Processor Intel ® Pentium ® 4
  • Memory 512 MB
  • Video Card VGA card with minimum 64 MB video RAM
  • Recommended PC Requirements
  • Operating System Windows Vista or Windows XP (SP2)
  • Processor Intel Pentium 4 (or later), 2.4 GHz
  • Memory 512 MB
  • Video Card VGA card with 128 MB video RAM
  • Remote Administration Full remote control through TCP/IP network