Access the Spectra IV camera menu using DS ControlPoint.

Issue

How to get into the Menus of the Spectra IV Ptz Camera (Preset 95) using DS ControlPoint.

How do I acces the preset 95 menu using Controlpoint.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint
  • Spectra IV
  • Spectra Mini
  • ExSite IP cameras

Cause

Access the camera menu to configure Spectra IV settings.

Resolution

 Preset 95

  1. Select the Spectra camera from the Systems camera tree.
  2. Select the Joystick Icon at the top of the screen.
  3. Use the drop down arrow and select 95 or just type in.
  4. Click on the SET button to enter the program menus of the camera.
  5. Use the control arrows to navigate the camera menu, Iris open to select.