Issue
Is it possible to install the Webstation server on a PC which don't have Vista installed?
Product Line
TAC Vista
Environment
Vista Webstation 5.x.x
Cause
Sometimes a customer like to install the Webstation server on in a DMZ for security reasons.
The purpose of a DMZ is to add an additional layer of security to an organization's local area network (LAN); an external attacker only has access to equipment in the DMZ, rather than any other part of the network.
Resolution
The Webstation server should be installed on a PC with TAC Vista installed.
But you can install a empty Vista server and connect it in a Vista network with the already installed Vista servers.
And then install the webstation server on the PC with the empty Vista server.