How to get into the menus using coaxitron or RS422 on the BU6 and the C20 DW series cameras

Issue

The current manual does not tell how to get into the menus of the C20-DW or BU6 when connected through coaxitron or RS422

Product Line

Pelco Cameras, Pelco Video Management, Pelco Matrix, Pelco Transmission & Power

Environment

  • BU6 and C20 -DW/CH series cameras
    • Pelco D RS422 control
    • Built in support for Coaxitron control

Cause

The current manual does not show how to get into the menu when connected through coaxitron or RS-422 (Pelco D only)

Resolution

 ACCESSING MAIN MENU (PRESET 95)

You can call up the main menu on your monitor by programming (setting or creating) preset 95 (28 if in 32-preset mode). Programming preset 95 for Pelco’s controllers varies according to the type of controller you are using. Instructions for programming preset 95 are given below for various Pelco controllers.

CM6700

  1. Enter the number of the camera and press the CAM key.
  2. Enter 95 and hold the PRESET key for two seconds.
  3. In the Edit Preset menu, arrow to SET and press the ACK key. The main menu appears.

KBD200A/KBD300A (Direct Mode Only)

  1. Enter 95.
  2. Hold the PRESET key (approximately 5 seconds) until the main menu appears on the screen.

CM8500

  1. Enter the number of the camera and press the CAM key.
  2. Press the ENTER button to prompt Menu Bar that should display along top of screen.
  3. Highlight CAM from the Menu Bar. A new drop down menu should appear.
  4. Highlight PRESET in the Camera menu and hold down the joystick button until the Set Presets prompt appears.
  5. Enter 95 and press the PRESET key. The text editor appears. Select ENTER and the main menu appears.

CM9500

  1. Enter the number of the camera and press the CAM key. The Main menu appears.
  2. Highlight SETUP in the Main menu and press the SELECT key.
  3. Highlight CAM in the Setup menu and press the SELECT key.
  4. Highlight PRESET in the Camera menu and press the SELECT key.
  5. Enter 95 and press the F1 key. The main menu appears.

CM9750

  1. Turn the KEY SWITCH to the ON position.
  2. Press the PROG key. PROGRAM appears on the LCD display.
  3. Press the PRES key. The PRESET prompt appears.
  4. Enter 95 and press the ENTER key. The main menu appears.
  5. Turn the KEY SWITCH to the OFF position.

CM9740/CM9760/CM9770

  1. Press the ESCAPE key to open the Main menu. Select DEF. The Define Menu appears.
  2. Enter your four-digit PIN if this is your first time entering this mode.
  3. Enter 95 and select PRST. The main menu appears on the monitor.
  4. Select the Quit icon to return to the default menu.

KBD4000/KBD4002/KBD4000V

  1. Press the SPOT MONITOR key.
  2. Enter 95, and then hold the PRESET key (approximately five seconds) until the main menu appears on the screen.

MPT9500

Standard Coaxitron® Mode

  1. Enter 95 and press the PRESET SET key.
  2. Position the asterisk in the YES row and press the F1 key. The main menu appears.

Extended Coaxitron or RS-485 Mode

  1. Enter 95 and press the PRESET SET key.
  2. Press the F2 key. The main menu appears.


BU6 Menu:


 


Note feature:

  • For coaxitron control no setting need to be done on the BU6. Coaxitron is built in.
  • Using coaxitron or D protocol will allow you to control the camera menu thru a pelco controller
  • The lens camera can be adjustment thru the camera menu when using Coaxitron or D protocol.