How do you navigate the menus once you are in them for the BU6 or the C20-DW series cameras

Issue

The current manual is not very clear regarding how to navigate the menus once you are in them

Product Line

Pelco Cameras, Pelco Video Management, Pelco Matrix, Pelco Transmission & Power

Environment

BU6 series cameras

C20-DW series cameras

Pelco D or coaxitron

C20-CH-6

Cause

The manual is not clear regarding the navigation of the menus when you are in them

Resolution

You navigate the menus the same as you would Spectra IV or Esprit. If in RS-422 Pelco D  or Coaxitron mode you would use Preset 95 to get into the menu and go through the menu settings by either joystick or mouse control as you would the Spectra series. The selections are outlined in the BU6 and in the C20-Dw manuals on Pelco.com.