Issue
Which object attributes are exposed on Vista's OPC server?
Environment
TAC Vista OPC server 1.6.X
TAC Vista Server 5.1.X
Cause
A user may wish to edit objects such as TAC Vista time schedules and force physical Xenta outputs from an OPC client?
Resolution
By default, all objects and all object attributes are exposed on the Vista OPC server. This can be controlled with authority and user settings.
Example of exposed Time Schedule attributes, shown in an OPC client.
Example of Time Schedule time event string, shown in an OPC client.
Example of exposed Xenta output attributes, shown in an OPC client.