Issue
What is the BACnet address and BACnet object ID for the Xenta 913?
Environment
TAC Xenta 913
Cause
The Xenta 913 does not have those features since it's not a BACnet device.
Resolution
The Xenta 913 is a gateway that translates the BACnet objects so that they can be read by for example Lonworks devices. It is not a
native BACnet device itself, hence it doesn't have a BACnet address or a BACnet object ID.