Quality of tubes delivered with the SPD 310/360 series sensors

Issue

What quality spec does the tubes included with the sensors have?

Product Line

Field Devices

Environment

004700320 SPD310-100/300/500/1000Pa
Differential Air Pressure
Transmitters
SPD310-100/300/500/1000Pa
 

004700340 SPD310-1000/1200/2500/5000Pa
Differential Air Pressure
Transmitters
SPD310-1000/1200/2500/5000Pa
 

004700360 SPD360-300/500/1000/2500Pa
Differential Air Pressure
Transmitters
SPD360-300/500/1000/2500Pa

Cause

The quality of the sensors are, depending on environment where installed, vital information in order to determine if the sensor is suitable or not.

Resolution

 

The included plastic tubing consists of the tubes and connection hose.
Tubes are from ABS Resin and the hose is from PVC.

Both materials themselves are suitable for a wide range of applications also outside and of high consistency against different influences.
But they are not especially strengthened against UV radiation.