When UltiVist completes a backup, where is the backup file stored?

Issue

When UltiVist completes a backup, where is the backup file stored?

Product Line

TAC I/A Series

Environment

UltiVist

Cause

For copying to portable media and safekeeping offsite.

Resolution

The backup file is located in the \FI\UVDBSAVE folder. 
The backup file is named:  UVBACK01.ZIP or UVBACK02.ZIP or UVBACK03.ZIP

UltiVist will create one file each time a backup is done.  It will overwrite one of the three files above so that there will only ever be three backup files in this directory.