Issue
How many BACnet MSTP trunks are supported on a Jace-600 and Jace-700?
Environment
Jace-600
Jace-700
Niagara G3
Cause
Job estimate requires a high number of BACnet controllers
Resolution
The Jace-600 and Jace-700 are capable of up to 5 BACnet MSTP trunks each: one on the main board, and four more if the two option cards are both installed (part# TRD-NPB-2X-485).
Only one MSTP driver is required to enable all five (part# ENC-DRV-MSTP).