Can more than four T-IO-16 I/O modules be added to the JACE-6 or JACE-6E hardware platform?

Issue

Can more than four T-IO-16 I/O modules be added to the JACE-6 or JACE-6E hardware platform?

Product Line

TAC I/A Series

Environment

I/A Series G3, JACE-6, JACE-6E, T-IO-16, T-IO-34

Cause

The JACE-6 controller will only recognize four I/O 16 modules.

Resolution

The JACE-6 and JACE-6E can only support ...

  • Maximum of four IO-16 modules or
  • Maximum of one IO-34 and two IO-16 modules