With an ASC controller, why does the MCI-Occ point cycle On/Off within 1-minute after pressing the Override button during the after hours schedule. An override period of 60-minutes is being used.

Issue

With an ASC controller, why does the MCI-Occ point cycle On/Off within 1-minute after pressing the Override button during the after hours schedule. An override period of 60-minutes is being used.

Product Line

TAC I/NET

Environment

I/NET Site

Cause

With an ASC controller, why does the MCI-Occ point cycle On/Off within 1-minute after pressing the Override button during the after hours schedule. An override period of 60-minutes is being used.

Resolution

Check to ensure the setup/setback features within a Temperature Control extension (attached to the MCI-Occ point) are not populated. Only use the setup/setback features within the ASC Parameter editor.