Atlas firmware version 1.02.0016 is not holding static IP address.

Issue

The TXB-IP will not retain a static IP address and sometimes other settings will not be retained. Also changes to the IP address will not apply.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Version 1.02.0016
  • Spectra Mini IP
  • Spectra IV IP
  • TXB-IP

Cause

Firmware version 1.02.0016 does not accept static IP address changes. Additional programmable settings may or may not take.

Resolution

A new version of Spectra Mini IP firmware version  01.02.0018c has been posted on Pelco.com or can be downloaded here: https://schneider-electric.box.com/s/dmckc4j9jp3p69li67daljjv6et05x2w

Use of Endura Utilities is recommended and may be downloaded from the following published article: LL#12584