Configuring Pelco Analytics (Video): Object Counting

Issue

Information to assist with the configuration of Pelco Analytics Object Counting

Product Line

Pelco Video Management

Environment

  • Sarix Legacy
  • Sarix Enhanced
  • Sarix Professional
  • Pelco Analytics
  • Object Counting

Cause

Calibration of Pelco Analytics Object Counting

Resolution

There are four steps needed to set up a Object Counting behavior in a web browser:

1. Configure the behavior on the EVENTS TAB => Analytic Configurations.
2. Configure the Behavior as a trigger in SOURCE
3. Set as an action in HANDLER
4. Select the EVENT STREAM in Primary Streams to view in a browser.

Video of how to configure Pelco Analytics Object Counting using a Sarix camera. 

 
For additional videos please see http://www.youtube.com/user/pelcobrian

 

Keyboard shortcuts for Sarix IP cameras