Is an IP camera license required for each analog camera connected to the DSSRV via the ENC5416, ENC5516?

Issue

Is an IP camera license required for each analog camera connected to the DSSRV via the ENC5416?

Product Line

Pelco Video Management

Environment

  • DSSRV
  • ENC5416
  • ENC5516
  • DS License

Cause

Product Specification - Spec Sheet.

Resolution

No. The DSSRV does not require IP Camera Licenses for any analog camera connected to an ENC5416, ENC5516 video encoder.  IP camera Licenses are only required for any IP camera added to the DSSRV.