Can more than 25 browser sessions be supported by Web Client?

Issue

Over 25 user Web Clients are required

Product Line

Andover Continuum

Environment

Web Client

Cause

Web Client licenses are only available for 1 , 2, 5, 10, 15, 20, or 25 users

Resolution

Each Web Client session can support up to 25 concurrent browser sessions, for a large system that requires additional sessions additional Web Client servers can be used, each supporting up to 25 Users.

Each Web Client server however will have a different IP address / URL, so if a user finds one server fully utilized, they will then need to connect to a different server/ address to connect to the system.

Also see Lessons Learned #6801 for information on Licensing.