DX4700/4800 Alarm/Motion features and DS Control Point

Issue

Will the DX4700/4800 Alarm/Motion recording indicators work on the DS Control Point software?

Product Line

Pelco Video Management

Environment

  • DX4700
  • DX4800
  • DS Control Point

Cause

The alarm and motion recording indicators from the DX4700/4800 do not display on the DS Control Point program.

Resolution

At this time, these features are not available.