Part numbers for the XMUX2 16/32 and XMUX2 Cable.

Issue

XMUX2 and connecting cable part numbers.

Product Line

Pelco Video Management

Environment

  • DVXi
  • DVXe
  • DS XPress

Cause

Part numbers for Xmux2 and data cable.

Resolution

The part# for the XMUX2 16 is 3326-10001.
The part# for the XMUX2 32 is 3327-10001.
The part# for the connecting data cable from the XMUX2 to the Integral DVR/HVR is 6990-00172.

Note: These are obsolete and can no longer be purchased.