Copy Files to Linux Devices Using Utilities

Issue

Copying files to linux devices.

Product Line

Pelco Video Management

Environment

  • Endura
  • SM5000
  • NSM5000
  • EE500
  • Sarix
  • VCD5202
  • NET5402R-HD
  • NET5404T

Cause

File transfer to Linux device is needed to resolve/implement solution.

Resolution

1. Open and Log into Endura Utilities.

2. Right click on the device and Select SCP and then the Copy files to Option.

3. You will then be prompted to select the file you are copying to the selected device. Browse for the file and select the desired file to be copied.

4. At the next prompt, you will have to specify the path in which the file is copied to.  **NOTE: In this example we are copying the file to /root, you may use any path desired here.