Can the DX Series Client playback exported video from the DX8100 Series HVR or DX8000 DVR?

Issue

Can the DX Series Client playback exported video from the DX8100 Series HVR or DX8000 DVR? 

Product Line

Pelco Video Management

Environment

  • DX Series Client - all version
  • DX8000 Series DVR
  • DX8100 Series HVR

Cause

Features is not supported by the DX Series Client.

Resolution

At this time the DX Series Client application cannot playback exported video from the DX8100 Series HVR or DX8000 DVR. Please refer to DX_Series_Client_Support_Features for which features are supported by the DX Series Client on each DX family product line. To play back exported video, use the DX8000/DX8100 Viewer.