Can the DS ControlPoint client software run on the DSSRV?

Issue

Using the DSSRV recorder as the viewing station for DS ControlPoint.

Product Line

Pelco Video Management

Environment

  • DSSRV
  • DS ControlPoint Client

Cause

A client PC is not available for use as a DS ControlPoint viewing station.

Resolution


While the DS ControlPoint client can be run at the server, doing so can impact performance of the DSSRV. For optimum performance, run DS ControlPoint at a client station.

Related Articles:

What are the minimum PC requirements for a DS ControlPoint remote client workstation?