Issue
Is there a limitation in number of lines in the TGML editor when running in source mode?
Product Line
TAC Vista
Environment
- Vista 5.1.8
- TGML editor 5.1.8
Cause
When a graphic is opened in the editor and Source mode is chosen it is possible to see the source code for the graphic and the number of lines in the source code.
Resolution
There is no known limitation on number of lines for a TGML graphic.