Enabling Auto-Reboot on Windows 7.

Issue

Recommended for all windows 7 systems.

Product Line

Pelco Video Management

Environment

Digital Sentry, DSSRV

Cause

Need to set up auto-reboot.

Resolution

  1. Launch Task Scheduler by clicking on Start and typing Task Scheduler.
  2. Click Action and select Create Basic task.
  3. Type AutoReboot or other preferred name by user in the Name box and click Next.
  4. Select Weekly and click Next.
  5. Type the time you want to restart the computer and click Next.
  6. Select Start a program and click Next.
  7. Click Browse and navigate to C:\Windows\System32 and select Shutdown.exe application and click Open.
  8. In the Add arguments (optional) box type –F –R and click Next.
  9. Click Finish.