Issue
Unifact Pro - Master and Slave controller ratio
Unifact Pro - Number of controllers on a LAN
Environment
Unifact Pro
Cause
What is the Master to Slave controller ratio of Unifact Pro controllers on a LAN?
What is the maximum number of Unifact Pro controllers on a LAN?
Download here the Unifact Pro Datasheet
Resolution
There is 1 master to a maximum of 3 slaves.
A single Unifact Pro LAN can support up to 80 controllers.
Note:
A S-Link sensor wired to the master can be shared by up to 3 slave controllers.
If fan speed control is used then S-Link sensors cannot be used on the slaves.