StruxureWare Building Operation Demo Database Package

Issue

StruxureWare Building Operation Demo Database Package

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation site

Cause

StruxureWare Building Operation Demo Database Package and going between releases.

Resolution

Global Demo Database Package V1.5 is currently not available. Please refer to the StruxureWare Building Operation v1.5 Sales Enablement Kit (A4)
Global Demo Database Package V1.4 is currently not available.

Global Demo Database Package V1.3.01 is available on The Exchange Download Center.
Because the database is installed using the “restore” process, the software must be the same exact version as used for the demo database backup files. Upgrading between versions is not supported.
Global Demo Database Package v1.2.01 is available on The Exchange Download Center.  Read the full Demo Database Package v1.2.01 Marketing Announcement for more information.

Note that the Demo Database package is a sales and marketing tool for your use “as is”. It is not a product supported through Product Support Services (PSS). If you have product specific technical issues such as installing the software applications (e.g. License Administrator, Enterprise Server) PSS may be able to help. However, PSS does not support the Demo Database contents or features. The Demo Database can be re-installed to return to its original state.