Issue
Some sites may want to have continuous recording at 1 fps (frame per second), motion at 10 fps and alarm conditions (live) at 30 fpx
Environment
Continuum
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
An attempt is made to find a place in Continuum where the frame rate can be edited, but the location of the feature cannot be found.
Resolution
There is no place in Continuum to adjust the frame rate per second for different features for Digital Sentry or Endura.
The only adjustment that can be made in Continuum is that on record video playback, the fast forward button can clicked several times in order to move faster. To go back to normal speed click the play button again.
All other frame rate adjustments have to be made in DS admin for Digital Sentry or in Endura.